Set up connections for a list indicator
Use the
Connections
tab of the List Indicator Properties
dialog box to set up a tag or expression for the object.To set up tags and expressions for a list indicator
- In theGraphics Displayeditor, double-click the indicator to open itsPropertiesdialog box.
- Click theConnectionstab.
- Assign a tag or expression to this connection:IndicatorA read connection. You can assign a tag or an expression to this connection. If you assign this connection, the object does not display the value sent to the Value connection until it receives a response from the Indicator connection.If you assign a tag, the application reads the value of the tag at the data source, assigns this value to the connection, and updates the object in the display to reflect the state corresponding to the value or least significant bit value (depending on the trigger type).If you assign an expression, the application calculates the value of the expression and updates the object’s display to reflect the state corresponding to the value or least significant bit value (depending on the trigger type).
Provide Feedback