Causes of runtime errors for a list indicator
At runtime, these circumstances produce these error conditions:
Invalid values
If the Indicator connection value does not match any of the state values for the indicator, none of the states in the list are highlighted.
Unassigned connections
If the Indicator connection is not assigned, none of the states in the list are highlighted.
Provide Feedback