How the list indicator works at runtime

The list indicator displays a configured list of states for a process or operation, and highlights the current state. The current state is the state in the list whose value matches the Indicator connection value at the data source (if the Trigger type is set to
Value
on the
General
tab) or the state whose value matches the value of the least significant bit set high in the Indicator connection at the data source (if the Trigger type is set to LSB).
TIP:
  • If the value (or the least significant bit value) of the Indicator connection does not match any of the configured state values for the list indicator, none of the states are highlighted.
  • If an array tag is assigned to the object's Value connection, and the Trigger type is set to Value, none of the states are highlighted. An error message will be shown.
Use controls
If the Indicator connection value is a floating point value, the application rounds the value to the nearest integer to determine the state to display.
Open graphic displays
  • When you open a display at runtime, the application reads the Indicator connection value and updates the display based on the value and the trigger type.
  • If there are more states than fit in the list, the application scrolls the list to display the current state.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal