Set up the Timing tab for a Key button
If you set up auto repeat, when the operator presses and holds down the
Key
button, repeated button presses are registered until the operator releases the button. You can set up auto repeat for the Move Up
, Move Down
, Move Left
, Move Right
, Page Up
, and Page Down key
buttons.To set up auto repeat for a Key button
- In theGraphics Displayeditor, double-click the object to open itsPropertiesdialog box.
- Click theTimingtab.
- Specify the auto repeat settings to use with theKeybutton.
Provide Feedback