Causes of runtime errors for a Key button

If a
Key
button's
Send Press To
property is set to
Linked Object
, and the object specified in the
Linked Object
property does not exist, or is not a valid object for the
Key
button to work with, when the button is pressed, the application logs an error to the diagnostics.
For details on the error conditions that occur when a Key button function is sent to the selected object, see the help for the object you’re using the
Key
button with control list selectors and display list selectors.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal