How the Key button works at runtime
The
Key
button’s behavior at runtime depends on which other objects appear on the display with the Key
button, and whether the Key
button's Send Press To
property is set to Object With Focus
or Linked Object
.Key
buttons do not work with all objects. If a Key
button's Send Press To
property is set to Object with Focus
, but the object with focus on the display does not work with the Key
button, when the operator presses a Key
button, nothing happens.If a
Key
button whose Send Press To
property is set to Object with Focus
is pressed, and there is no selected object, nothing happens.Provide Feedback