Set up general properties for a Key button
Use the
General
tab of the Key Button Properties
dialog box to set up how a Key
button looks.To set up general options for a Key button
- In theGraphics Displayeditor, double-click the object to open itsPropertiesdialog box.
- Click theGeneraltab.
- Specify the options.
Browse
button (...) in the Linked object
field to open the Object Browser
and select the object to link to.Once you set up the options on the
General
tab, click the Label
tab to specify a caption or image for the button.Provide Feedback