How the display list selector works at runtime

The display list selector shows a list of graphic displays that the operator can choose from. The operator can move through the list and select a graphic display. When the operator presses
Enter
, the selected display opens.
The operator can scroll through the list and select displays using key buttons or by using the arrow keys and the
Enter
key on a keypad or an external keyboard.
The display list selector’s behavior at runtime also depends on which types of graphic displays are already open and which type of display is opening.
Use display types
  • If the selected graphic display is a Replace display, it closes any open On Top or Replace displays. It does
    not
    close any On Top displays that use the
    Cannot Be Replaced
    option.
  • If the selected display is an On Top (with or without the
    Cannot Be Replaced
    option), the display is positioned using the graphic display’s settings.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal