Causes of runtime errors for a display list selector

At runtime, the selected display does not open and the application logs errors about the display list selector to diagnostics if:
  • The selected display has been deleted from the project.
  • The operator does not have security access for the display.
  • The selected display is the display that contains the display list selector.
  • The display change is controlled remotely (by the data source) and a Replace display is assigned to the list item the operator has selected.
  • The parameter file specified has been renamed or does not exist.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal