TerminalWakeUp ActiveX control

The TerminalWakeUp ActiveX control provides the system with the ability to wake up or exit from screen saver mode when the control is triggered.
Use the TerminalWakeUp ActiveX control to:
  • Read the terminal IP address as a string
  • Read the individual terminal IP address octets as a separate value
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal