TerminalInfo ActiveX control
The TerminalInfo ActiveX control allows an HMI application to read the following
PanelView Plus 7
and PanelView Plus 6
hardware attributes and write the values to tags:- CPU Temperature
- Logic Board Temperature
- Display Temperature
- Battery Voltage
- CPU Load
- Memory Load
- Memory (BinFS) Thrashing
- Device Name
- Internal NIC IP Address
- Internal NIC Subnet Address
- Internal NIC Gateway Address
- Internal NIC MacID
- External NIC IP Address
- External NIC Subnet Address
- External NIC Gateway Address
- External NIC MacID
The TerminalInfo ActiveX control also provides the ability to read certain information of personal computers, such as IP addresses.
Provide Feedback