SBCP ActiveX control

The SBCP (Set Bit Cursor Point) ActiveX control maps an integer value to one of a set of 100 tags. The 100 digital tags are mutually exclusive, and only one of the tags can be set to one (1) at any given time.
Use the SBCP ActiveX control to:
  • Set one tag out of 100 tags to one (1) based on an indexing tag's value to create state-based animation sequences for representing machine operation
  • Enable and disable the control at runtime under application control
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal