IPInfo ActiveX control

The IPInfo ActiveX control provides the system with the ability to read the hosting
PanelView Plus
terminal's TCPIP settings and certain information of personal computers.
Use the IPInfo ActiveX control to read:
  • Terminal or personal computer IP address as a string
  • Individual terminal or personal computer IP address octets as separate values
  • Terminal subnet mask address as a string
  • Individual terminal subnet mask address octets as separate values
  • Terminal gateway address as a string
  • Individual terminal gateway address octets as separate values
  • Terminal MAC ID as a string
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal