Popup keyboard definition file

A popup keyboard definition file is used to configure the popup keyboard keys.
A definition file has the following characteristics:
  • The file must be saved as Unicode text.
  • The definition file is tab-delimited.
  • The file can be stored on the internal or external storage card when using a
    PanelView Plus
    terminal. The use of a network drive is not recommended.
  • There is no limit to the number of key sets the file defines.
  • The first line of the definition file specifies the key set name. For example, "Default" "Set1" "Set2" "Set3".
  • Redefinition of the keys "Home", "End", "Page Left", "Page Right", "Spacebar", "ESC". "CLR", "<<", ">>", "<--", and "<--|" will be ignored.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal