Custom String Popup Keyboard ActiveX control
The Custom String Popup Keyboard ActiveX control provides the system with the ability to present the operator with a keyboard that is customized to the specific application running on a
MobileView
, PanelView Plus 7
, PanelView Plus 6
, PanelView Plus
, PanelView Plus Compact
, or PanelView Plus CE
terminal.Use the Custom String Popup Keyboard ActiveX control to:
- Configure keyboards for different languages, for example, Chinese, Korean, Japanese, French, and others
- Specify multiple key sets to configure the operation of the custom popup keyboard
- Use the user entry, created with the popup keyboard, in the HMI application
- Specify the length of the string returned from the popup keyboard
- Control when the popup keyboard is available to the operator
Provide Feedback