Automatically delete old data log files

If you select the
Periodic
option or the
At Specified Times
option on the
General
tab of the
ME CSVDataLog Properties
or the
ME DataStore Plus Properties
dialog box, you can automatically delete old data log files.
To automatically delete old data log files
  1. Double-click the CSVDataLog or the DataStorePlus ActiveX control to open its
    Properties
    dialog box.
  2. On the
    General
    tab, in the
    Delete Oldest Files
    area, select a check box for the options to be used and specify the settings to be applied.
    TIP:
    If you select both check boxes, files are deleted after the maximum time or after the maximum number of files is reached, whichever happens first.
  3. Click
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal