Start a new log file at a specified time
You may need to start a new log file at a specified time.
To start a new log file at a specified time
- Double-click the CSVDataLog or the DataStorePlus ActiveX control to open itsPropertiesdialog box.
- On theGeneraltab, select theAt Specified Timesoption.
- In theStart Timestext box, type the specific date and time combination for the new log file to start.Only one specific combination can be on a single line. Start a new line for an additional date and time combination.
- ClickOK.
Provide Feedback