Define global object parameters

Global object parameters are defined in base objects in global object displays. When you copy a global object from a global object display to a standard display in the
Graphics
folder, you can assign values to the global parameters in the resulting reference object.
To define global object parameters
  1. Right-click the base global object or global object group on a global object display and select
    Global Object Parameter Definitions
    . Alternatively, on the menu bar click
    Edit
    >
    Global Object Parameter Definitions.
  2. (Optional) In the
    Global Object Parameter Definitions
    dialog box, enter the description for each parameter.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal