Detect the integrity of a CSV data log file using the CSV Data Log Tamper Detection Utility
You can detect the integrity of a CSV data log file using the CSV Data Log Tamper Detection Utility.
To detect the integrity of a CSV data log file using the CSV Data Log Tamper Detection Utility
- In the CSV Data Log Tamper Detection Utility, select a CSV data log file and clickDetect.TheDetection Reportdialog box opens and shows the detection result.
- (optional) In theDetection Reportdialog box, clickSave Resultto save the report as a text file.
Provide Feedback