CSV Data Log Tamper Detection Utility
How do I open the CSV Data Log Tamper Detection Utility?
Use one of the following methods:
- From WindowsStartmenu, selectAll apps > Rockwell Software > Rockwell Automation CSV Data Log Tamper Detection Utility.
- InFactoryTalk View Studio, from theToolsmenu, selectRockwell Automation CSV Data Log Tamper Detection Utility.
Use the CSV Data Log Tamper Detection Utility to:
- Detect the integrity of a CSV data log file that contains tamper detection strings
- Generate a detection report when the detection is completed
- Save the detection report to a text file
TIP:
You can install this utility independently from the path
FTView-DVD\<version>-FTView\Tools\CSV Data Log Tamper Detection Utility
. It doesn't have any version dependencies on FactoryTalk View ME
.Saving changes to a CSV data log file in
Microsoft
Excel corrupts the file, and CSV Data Log Tamper Detection Utility cannot detect tampers in the file.Provide Feedback