Export text strings to an Excel spreadsheet
If an application supports multiple languages, you can export the text strings for all the application languages to a Microsoft Excel spreadsheet (*.xls). The following versions of Microsoft Excel are supported:
- Excel 2000
- Excel 2002
- Excel 2003
- Excel 2007
- Excel 2010
- Excel 2013
To export text strings in an application to an Excel spreadsheet
- In theLanguage Configurationdialog box, clickExport.
- In theExport Operationwindow, selectExport strings for all languages to an Excel spreadsheet.
- If you select theOptimize duplicate stringscheck box, the strings that appear repeatedly in the application appear only once in the spreadsheet, and need only be translated or edited once. When the file is imported, each instance of a duplicate string is replaced by the same edited or translated string.
- If you select theOpen exported filecheck box, the exported file opens as soon as the export is finished.
- Select a destination for the exported text strings.TIP:
- The default name for an exported Excel file is:<application name>_<export version number>.xlsFor example, Brewery_1.xlsThe first time you export strings to Excel, the export version number is 1. For each subsequent export from the same application, the number increases by 1.
- When you export strings to an Excel spreadsheet, undefined strings are exported as "**UNDEFINED**". If this is not replaced with a text string during the translation process, an undefined string will be imported into the application.
- For the instructions on opening a text file in Microsoft Excel, see "Set up language switching" in the.FactoryTalk View MEUser's Guide
Provide Feedback