Name a backup archive
When backing up an application, you need to name a backup archive.
To name a backup archive
- In theEnter a name for the application archivebox, type a name for the application you are backing up.The default name will be the name of the selected application.TIP:If the name is the same as an existing application, you will be prompted to overwrite the existing application. If you want to overwrite it, clickYes. If you do not want to overwrite it, clickNoand enter another name.
- Specify where to store the application archive. You can type the location, or click theBrowsebutton (…) to search for and select the location.The default location for backup archives is\Users\Public\Public Documents\RSView Enterprise\ME\Archives
- If you want to protect your backup files with a passphrase, select theEncrypt file contentscheck box.You will be required to enter the passphrase when you restore any backup file that is passphrase protected.TIP:If you do not wish to encrypt the backup file contents, it will be saved as a plain text backup file.
- If you selected theEncrypt file contentscheck box, type a passphrase and enter it again in theConfirm passphrasebox.
- ClickFinish.
All application configurations including
FactoryTalk Services Platform
/System, as well as the physical project folders of the HMI server, are backed up.Provide Feedback