Set up recipe units (Units tab)

Use the
Units
tab to pair tag sets with data sets to create recipe units.
When a new recipe is created, a new recipe unit with the default name of Unit 1 is created, pairing the default data set Data Set 1 and the default tag set Tag Set 1.
Click on a unit name to select it. You can then edit the selected unit, delete the selected unit, or insert a new unit at the bottom of the list.
Options
  • Unit name
    Click on a unit name to select the unit. The Data Set and Tag Set are automatically selected as part of the unit.
    • Insert
      Click this button to open the
      Insert Unit
      dialog box.
    • Edit
      Click this button to open the
      Edit Unit
      dialog box.
    • Delete
      Click this button to delete the selected unit.
      TIP:
      • Double-click on a unit name to open the
        Edit Unit
        dialog box.
      • Press the
        Delete
        key to delete the selected unit.
      • Rename a unit by clicking and holding on the unit name.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal