Select displays to export

Choose which of the displays in your application you want to export as XML files. By default, all the displays are selected for export (checked).
To select displays to export
  1. Clear the check boxes for those displays you do not want to export.
  2. Click
    Next
    .
Options
Select the displays to export
The list displays all the displays in your application, including default displays.
  • Select All
    Click this box to select all the displays for export. By default, all the displays are selected.
  • Clear All
    Click this box to clear the check boxes for all the displays in the application. When you clear all the displays, the Next button becomes unavailable.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal