Select an export folder
Select the folder where you want the exported graphics XML files stored. By default, these files are exported to the
My Documents
folder.To accept the backup location, click
Next
.To select a new export folder
- Click theBrowsebutton to open theBrowse for Folderdialog box.
- Select a folder from the tree, or create a new folder.
- To create a new folder, navigate to the location for the new folder. ClickMake New Folder, and then rename the new folder.
- When you have selected a folder, clickOK. The folder name and the path to its location appear in the text box.
- ClickFinish. The selected graphic display files are exported to the folder as XML files.
Provide Feedback