Select a backup folder

Select the folder where you want the backup graphic files stored. The backup copies are made and stored in this location when the
Finish
button is clicked, just before the file or files are imported.
By default, the application stores these files in the folder
My Documents
. To accept the backup location, click
Next
.
To select a new backup folder
  1. Click the
    Browse
    button to open the Browse for
    Folder
    dialog box.
  2. Select a folder from the tree, or create a new folder.
  3. To create a new folder, navigate to the location for the new folder. Click
    Make New Folder
    , and then rename the new folder.
  4. When you have selected a folder, click
    OK.
    The folder name and the path to its location appear in the text box.
  5. Click
    Next
    . The
    Import File Type
    dialog box opens.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal