Back up graphics displays before an import
When you select the import operation in the
Graphics Import Export Wizard
, you are offered an opportunity to make backup copies of the files that will be overwritten when the selected files are imported. By default, Yes
is selected.Backup copies of graphic displays are stored as .gfx files.
Options
- YesChooseYesto create backup copies of the selected files. When you clickNext, theBackup Folderdialog opens.
- NoChooseNoto overwrite the files in the application with the files being imported. When you clickNext, theImport File Typedialog opens.
Provide Feedback