Rename a component
The following components can be renamed:
- Displays
- Libraries
- Images
- Parameters
- Local Messages
- Information Messages
- Data log Models
- Macros
To rename a component
- Select the component in theExplorerwindow.
- Right-click the component and selectRename.
- In theRenamedialog box, type the new name in theTotext box.
- ClickOK.TIP:The rename function changes the component name shown in theExplorerwindow and the file name listed in Windows Explorer.Rename components withinFactoryTalk View Studio. Do not rename files using Windows Explorer.A component name and its path can be up to 256 characters.
Provide Feedback