Remove a component
Removing components removes them from the
Explorer
window but leaves them on the hard disk.To remove a component
- InFactoryTalk View Studio, in theExplorerwindow, right-click the editor icon and selectRemove.
- In the component selection dialog box, select the components to be removed and clickOK.
- Click theYesbutton to confirm the removal.TIP:To remove a component, you can also right-click the component in theExplorerwindow and selectRemove.
Provide Feedback