Filter a component
Filter a component to show only the ones that meet the specific criteria in the Explorer window. You can filter:
- Displays
- Global Objects
- Parameters
- Computers and Groups
- Networks and Devices
- Users and Groups
The filter applies to the current application only. Reopening the application or opening a new one will clear the filter, and all the components show in the Explorer window.
To filter a component:
- In the Explorer window in FactoryTalk View Studio, right-click a component (for example,Displays) that you want to filter, and then clickFilter.
- In theFilterdialog box, select a filter condition, and then enter a filter term.
- ClickOK.A filter icon appears beside the component. The filtered components remain in their original folders.TIP: To clear the filter, right-click the component, and then clickClear Filter.
Provide Feedback