Delete a component
Deleting components deletes them from the
Explorer
window and from the hard disk.To delete a component
- InFactoryTalk View Studio, in theExplorerwindow, right-click the editor icon and selectDelete.
- In the component selection dialog box, select the components to be deleted and clickOK.
- Click theYesbutton to confirm the deletion.TIP:To delete a component, you can also right-click the component in theExplorerwindow and selectDelete.
Provide Feedback