Disable optimization for dynamic links manipulated at runtime
If you optimize a project, you must manually disable optimization for dynamic links
that are manipulated at runtime
- InProject view, select the project variable with the dynamic link.
- InProperties, select.
Change Dynamic Link - SelectAdvancedand then select
Settings. - SelectRuntime optimizationand then selectDisabled.TIP: You can also right-click the dynamic link inPropertiesand select . To enable optimization, selectEnable optimization.
Provide Feedback