Optimize a project
Improve performance at runtime by optimizing your project. Optimized dynamic links
and tags improve navigation speed between screens in a FactoryTalk Optix Application and
widgets at runtime. Tags are optimized in a project by default, but dynamic links are not
optimized by default.
- To optimize dynamic links for a project, inProject view, select the project node.
- InProperties, expand theRuntime optimizationcategory.
- InDynamic links, selectTrue.
- By default, tags are optimized. To disable tag optimization, inTags, selectFalse.
Dynamic links and tags are optimized for the project. When you
optimize dynamic links for a project, you must Disable optimization for dynamic links manipulated at runtime.
Provide Feedback