Drawing tools

Use drawing tools in the editor to display custom shapes at runtime.

Shapes

You can draw one-dimensional shapes including:
TIP: To display or hide the grid, change the grid size, and prevent a drawing from snapping to the grid, see Configure the editor grid.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal