FactoryTalk Optix Studio web editor
You can use
FactoryTalk Optix Studio
in a web browser through FactoryTalk Hub
.Editor features support
FactoryTalk Optix Studio web editor
supports all FactoryTalk Optix Studio desktop editor
features
except for: - Save logs from theOutputtabs.
- Edit NetLogic files.
- Display paths in logs in theOutputtabs.
- Add files and images by dragging and dropping them intoFactoryTalk Optix Studio web editor.
- Restart the application at runtime by using the method.
Emulator features support
FactoryTalk Optix Studio web editor
emulator supports all features of FactoryTalk Optix Studio desktop editor
emulator except for: - Control theWebBrowserobject in the runtime emulator.
- Control thePDFViewerobject in the runtime emulator.
- Control theVideoobject in the runtime emulator.
- Control theWindowobject in the runtime emulator.
- Cursor does not indicate areas in which you cannot drop elements.
Change to the ImagePosition property for a button
The data type for the
ImagePosition
property changed to ButtonImagePosition
. Any existing NetLogic scripts that assign a value to Position
need to be changed to ImagePosition
.Provide Feedback