Application notes
These application notes apply to
FactoryTalk Optix
version
1.6.x.Threat mitigation
- Do not lose the USB Key with exportedFactoryTalk Optix Application. The USB key contains inspectable fields, credentials, certificates, and hashed passwords.
- Protect physical access toRockwell Automationmanufactured devices.
- Do not leave connected devices unattended. Protect physical access to the device and protect logs from device web interface, connected diagnostic session, and file system access via remote assistance tool.
- Prevent unauthorized physical access to the device. Protect physical access to the device and improve security level of application files generated by custom logics.
- Protect physical access to logged-in user sessions. Prevent the theft ofFactoryTalk Hubrefresh token file by locking the session if unattended.
- Protect physical access to logged-in user sessions. Prevent the removal ofFactoryTalk Hubrefresh token file by locking the session if unattended.
- Protect physical access to logged-in user sessions. Prevent attacks while logging in to GitHub.
Feature preview
Features labeled as preview should not be used in a production environment. Feature preview includes:
- RA EtherNet/IP communication driver in the FactoryTalk Optix Studio web editor and Emulator
- Connected IDE mode
- Contents of Feature Preview library folder
- Model analysis providing information model graphs
Spinbox Numeric Input unsigned conversions
When the Spinbox datatype is an unsigned integer, negative inputs are converted to zero.
Mouse Up Event modified behavior
The Mouse Up Event is now executed only when removing the pointer or finger while remaining inside the UI object area. This modification affects the UI controls Panel, Rectangle, Button, Ellipse, Polyline, Image, and AdvancedSvgImage. A new variable related to the pressed status will be included in a future release.
Incorrect status under Micro Controller Driver
When multiple stations are configured, if there is no demand for data the connection status for the station is not updated. To avoid this situation, implement a heartbeat for each station using a runtime Netlogic script to clear a boolean when it is true, and a timer in the station that runs when the boolean is false and sets it to true when the timer completes.
Alarm limits
Device RAM | Optix Alarms,
Logix Tag-based Alarms, and Logix ALDM Instruction Alarms | Logix ALMA Instruction Alarms |
|---|---|---|
1 GB | 2500 | 400 |
2 GB | 5000 | 800 |
4 GB | 15000 | 1600 |
8 GB | 30000 | 3200 |
16 GB | 60000 | 6400 |
Device RAM | Optix Alarms,
Logix Tag-based Alarms, and Logix ALDM Instruction Alarms | Logix ALMA Instruction Alarms |
|---|---|---|
1 GB | 700 | 150 |
2 GB | 1000 | 200 |
4 GB | 3500 | 500 |
8 GB | 7000 | 1000 |
16 GB | 14000 | 2000 |
NOTE:
If your application uses Logix ALMA instruction-based alarms mixed with other types of alarms, count each ALMA alarm as 5 alarms. For example, if the FactoryTalk Optix application has 100 ALMA alarms and 2000 other alarms, the total number of alarms is 2500. Per the table above for a single local language, this is the quantity of alarms that will run inside 1GB with a normal application.
As shown on the table above, each local language requires additional memory. The additional memory required will be reduced in a future release.
If you are not using the new Alarm Manager or Alarm Summary counters, or if you are upgrading from a previous version of FactoryTalk Optix that does not require the new Alarm Manager or Alarm Summary counters, you can reduce the memory required by disabling alarms collection by setting the
Enable alarms collection
property to False
. Logix extended properties must define both Min and Max range
When importing Logix extended properties, both Min and Max must be defined in Logix and must
contain valid values in order for the extended properties to be imported.
Scroll bars
Dragging the scroll bar of rotated UI objects does not work as expected.
Method order
The order in which methods are performed changed in version 1.6.0 and may impact previous
applications migrated to version 1.6.0. If this occurs, you will need to update your
project.
Unsupported Mysql_native_password authentication plugin
The ODBC database store has been upgraded to use the MySQL ODBC connector version 9.2.0.0
which no longer supports the mysql_native_password authentication plugin.
To work around this issue, in the settings for MySQL Server, open
Users and
privileges
and change Authentication Type
to caching_sha2_password
.Enhanced Alarm Banner
In FactoryTalk Optix version 1.6.0, the Alarm Banner widget is enhanced to improve runtime
operation stability and performance. If you have a project that was created using a previous
version of FactoryTalk Optix and that has an Alarm Banner widget, you must use the upgraded
Alarm Banner widget. First, using FactoryTalk Optix version 1.6.0, open or upgrade a project
that was created with a previous release of FactoryTalk Optix. Next, remove the Alarm Banner
widget from your project. Finally, add a new Alarm Banner widget to the project from the
FactoryTalk Optix 1.6.0 template library.
OPC UA Recursive Models
The introduction of OPC UA Structures in 1.6.0 required the enforcement of stricter
modeling rules. These modeling rules may prohibit importing any OPC UA model that contains a
recursive reference, which is any type definition that contains a reference to itself.
Support for recursion is planned for a future release.
Provide Feedback