Develop an archives manager
    Use the preconfigured Zip Unzip NetLogic to create, extract, and password-protect ZIP archives.
Example application

     TIP: 
    
You can download a sample project from:
 ArchivesManager.zipPrerequisites
Select  to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
  to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
Run
Provide Feedback