Add a client device
    Configure a client device to allow the deployment of 
FactoryTalk Optix Applications
 over the network.- From the main toolbar, next to, select the client dropdown menu.Run
- (optional) InClient device settings, to display only the active remote client devices, toggleActive remote devices.TIP: Refresh remote client devices by selectingRefresh.
- Select either:- A folder and select. 
- AFactoryTalk® Remote Access™device and selectto add a device accessible from the selected FactoryTalk Remote Accessdevice network. FactoryTalk Remote Accessdevice network.
 
- (optional) InName, edit the name of the target device.IMPORTANT: Only alphanumeric characters are allowed in the name.
- InIP Address, enter the IP address of the target device.
- InUsername, enter the name of the user to log on to the target device.- Windows®username
- A system username:- DOMAIN\, for domain users.username
- , for local users on domain-joined devices..username
- , for local users on devices that do not belong to a domain.username
 
- Linux username
- An administrator username.
 IMPORTANT: A password must be configured for the user on the target device.
- (optionaI)Destination Path, enter the path on the target device to deploy the application.TIP: The default deployment destination path is%localappdata%. Defining a custom path is useful when theC:\partition of the client device is write-protected.NOTE: You can deploy only one project. Therefore, any application previously deployed toDestination Pathremoves the path in the default destination, and any application previously deployed to the default destination removes theDestination Path.NOTE:Destination Pathis only forWindowsclient devices runningFactoryTalk Optixas an application.Destination Pathis not supported when deployingFactoryTalk Optixrunning as a service.
- (optional) SelectEncrypt project on deviceto encrypt the deployed project on the target device.For more information, see Project encryption on a client device.
- (optional) SelectDownload source project on deviceto download the source project on the target device.TIP: Downloading the source project on the target device enables you to upload the source project from the target device to the development computer later on. For more information, see Open a project.
- ChooseSelectto select the target client device.
Provide Feedback