Develop a gauge with a localized engineering unit
    Create a linear gauge that displays the current temperature in a format adjusted to the logged in user.
Application example - Celsius degrees (it-IT)

Application example - Fahrenheit degrees (en-US)

     NOTE: 
    
Download a sample project:
 LocalizedEngineeringUnitGauge.zipPrerequisites
- To develop the project
- Arrange the interface elements.
- Save the project.
Application design example

Select  to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
  to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
Run
Provide Feedback