Properties pane
    Use the 
Properties
 pane to display variables for the selected object. Property values change the appearance and display of that object at runtime.Properties pane columns
      
| Item | Name | Description | 
|---|---|---|
|  | Property name column | Navigate through the properties available for a selected object. Select any property and start typing the name of the property to find. | 
|  | Property value column | Edit property values. To edit the values of some properties quickly, select the value and start typing. The values may automatically complete as you type. | 
     TIP: 
    You can navigate through properties and values by selecting them with your mouse or by using the arrow keyboard keys.
Properties pane buttons
      
  | Item | Function | 
|---|---|
|   Group by category | Organize the properties by category. | 
|   Sort alphabetically | Sort the properties in alphabetical order. | 
|  Add new | Add a property to the node. Add a display name, variable, alias, or audit signature.  In the  Eventscategory of the Properties pane, this button adds an event from the Eventsheader or a new method for the selected event. | 
| Delete | Remove an added property from the  Properties pane or reset the value of a default property. Delete the selected method in  Events. Deleting all methods from an added event deletes the event. | 
|   Detach view | Detach the pane from the main window. | 
|   Attach view | Detach the pane to the main window. | 
|  Open with editor | Open the editor for the selected object. This button is valid for only certain object types. | 
Property pane context menus
      To open the property context menu, right-click the property name.
        
  
    
| Item | Description | 
|---|---|
| New | Create child properties, variables, and aliases, or to create events based on the selected property. | 
| Delete | Delete properties, variables, and aliases. | 
| Copy | Copy child properties, variables, and aliases. | 
| Paste | Paste child properties, variables, and aliases. | 
| Collapse all | Collapse all children nodes of properties, variables, and aliases. | 
| Show References | Display which objects or variables reference the property. | 
| Copy path to node | Copy the path of properties, variables, and aliases in the project. | 
| Change modelling rule | Set the modelling rule:
                     
 | 
| Model analysis | Visualize the project information model in the form of a graph. See Display information model graphs. | 
To open the property value context menu, right-click the property value.
        
  
    
| Item | Description | 
|---|---|
| Copy | Copy the selected property value. | 
| Paste | Paste the copied property value to the selected property value. | 
| Reset Value | Reset the property value to the default value. | 
Provide Feedback