FactoryTalk Optix Studio interface
    Following is an example of 
FactoryTalk Optix Studio
 at design time. FactoryTalk Optix Studio components

| Item | Name | Description | 
|---|---|---|
|  | Project information model that displays the content and structure of the project in nodes. A node can be a parent that has child nodes.  | |
|  | Object types and variable types on which instances of objects are based. Predefined types are grouped in folders according to their purpose. Custom types are grouped in folders that reflect the structure in  Project view. | |
|  | Messages related to the operation of the  FactoryTalk Optix Application. Applications that are running and are connected to FactoryTalk Optix Studioappear on Emulator Output. | |
|  | Tabs | Tabs of open objects being modified in the editor. If you hover over a tab to select   without saving the project, you are prompted to save your changes. | 
|  | Editor toolbar | Commands that apply to the object type being modified in the editor.  | 
|  | Graphic editor for objects. Each editor opens in a new tab and is used for graphic objects and object types, such as tag importers and recipes. | |
Provide Feedback