Range Slider
Properties
Name | BrowseName | DataType | Description |
---|---|---|---|
Value change behavior | ValueChangeBehaviour | Mode of updating text when the user writes in the text box. At end of typing = update the value after the user has pressed Enter with either physical or virtual keyboard (pressing Esc or clicking outside the object, the previous text is restored); When typing = in real-time when writing. | |
Provide Feedback