Value change behavior

Mode of updating text when the user writes in the text box.
BrowseName
ValueChangeBehaviour

Values

Value
DisplayName
Description
0
Value change on edit finished
Update the value after the user presses Enter with either physical or virtual keyboard. Pressing Esc or selecting any area outside the object, restores the field text to its original value.
1
Value change while editing
The value is updated at the same time it is being modified.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal