Linear gauge

Set and/or display a whole number value within a range of possible values.
BrowseName
LinearGauge
SuperType
Element(Item)

Properties

Name
BrowseName
DataType
Description
Value
Value
Value displayed and possibly changed by the user.
Minimum value
MinValue
Minimum value displayed on the Y axis.
Maximum value
MaxValue
Maximum value displayed on the Y axis.
Major tick count
MajorTickCount
Quantity of main ranking signs.
Minor tick count
MinorTickCount
Quantity of secondary ranking signs.
Label visible
LabelVisible
Show/hide the scale values.
Editable
Editable
Enable/disable the change of the value directly in the chart.
Scale padding
ScalePadding
Value change behavior
ValueChangeBehaviour
Mode of updating text when the user writes in the text box. At end of typing = update the value after the user has pressed Enter with either physical or virtual keyboard (pressing Esc or clicking outside the object, the previous text is restored); When typing = in real-time when writing.
Scale position
ScalePosition
Position of the scale relative to the slider.
Orientation
Orientation
Horizontal or vertical orientation of the object.
Tooltip
Tooltip
Show/hide the value above the selection point.
Image path
ImagePath
Sets an image to be shown in place of the linear gauge bar.
Fill color
FillColor
Fill color of the linear guage bar.
Colorization mode
ColorizationMode
Set the colorization mode which will be used when applying the selected color to the image.
Warning zones
WarningZones
Ranges of values to display with a specific color.
Visible
Visible
(Inherited from Element)
Enabled
Enabled
(Inherited from Element)
Opacity
Opacity
(Inherited from Element)
Left margin
LeftMargin
(Inherited from Element)
Top margin
TopMargin
(Inherited from Element)
Right margin
RightMargin
(Inherited from Element)
Bottom margin
BottomMargin
(Inherited from Element)
Width
Width
(Inherited from Element)
Height
Height
(Inherited from Element)
Horizontal alignment
HorizontalAlignment
(Inherited from Element)
Vertical alignment
VerticalAlignment
(Inherited from Element)
Rotation
Rotation
(Inherited from Element)

Events

Modified value
BrowseName
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal