Wi-Fi configuration

Configure the Wi-Fi network interface.
BrowseName
WiFiConfiguration
SuperType
Object(BaseObjectType)

Properties

Name
BrowseName
DataType
Description
Operating mode
Mode
Adapter = the interface functions as a network adapter; Access point = the interface functions as an access point.
Network name
NetworkName
Network name (SSID).
Security mode
SecurityMode
Network security protocol.
Username
Username
(Only if Security mode = WPA2-Enterprise) Name of the user to connect to the network.
Security key
SecurityKey
Password to connect to the network.
Enable access to LAN network
EnableAccessToLanNetwork
Enable/disable access to the LAN sub-network for connected devices.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal