Wi-Fi modes

Wi-Fi interface operating mode (disabled/adapter/access point).
BrowseName
WiFiModeEnum

Values

Value
DisplayName
Description
0
Disabled
The Wi-Fi interface is disabled.
1
Adapter
The Wi-Fi interface is used to connect to an existing wireless network.
2
Access point
The Wi-Fi interface is used to create a wireless network.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal