Data logger
Samples values of one or more variables at regular time intervals or on command, and stores them in a database.
Properties
Name | BrowseName | DataType | Description |
---|---|---|---|
Sampling mode | SamplingMode | None: automatic recording disabled, can record by invoking the Sample method; Periodic: records the values of all the selected variables at regular intervals; Value change: at regular intervals records only the values of the selected variables that have changed with respect to the previous sampling. | |
Sampling period | SamplingPeriod | Interval in hours, with millisecond precision, between one sampling and the next, in the Periodic mode. | |
Polling time | PollingPeriod | Interval in hours, with millisecond precision, between one sampling and the next, in the Value change mode. | |
Log operation code of each variable | LogVariableOperationCode | (Only for reading of variables from a controller) Enable/disable the storage of the operation code for the reading of the controller. If enabled, adds the relative column in the database for each variable. | |
Log timestamp of each variable | LogVariableTimestamp | Enable/disable the storage of the timestamp of each sample. If enabled, adds the relative column in the database for each variable. | |
Log local time | LogLocalTime | Enable/disable the recording of the local date and time (Local time property of the events or session), in addition to the date and time in UTC+0. | |
Default deadband mode | DefaultDeadBandMode | (only for the Value change sampling mode) Method of calculating the change of values, with respect to the previous sampling, within which not to sample. Applies to all variables without specific deadband mode. None: any change; Absolute: absolute change of the values of the variables; Percentage: percentage change of the values of the variables. | |
Default deadband value | DefaultDeadBandValue | (only for the Value change sampling mode) Value of the deadband interval. For example, if the value is 5, the logger samples the variables whose values have had an absolute or percentage change of at least ± 5 with respect to the previous sampling. | |
Methods
Log
- BrowseName
- Log
Provide Feedback