Variable to sample
Variable to sample with a Data logger object.
Properties
Name | BrowseName | DataType | Description |
---|---|---|---|
Last operation result code | LastOperationCode | (Only for reading of variables from a controller) Operation code for the last controller reading. | |
Deadband mode | DeadBandMode | (only for the Value change sampling mode) Method of calculating the change of value, with respect to the previous sampling, within which not to sample. It has priority over the logger deadband general mode. None: any change; Absolute: absolute change of the values of the variable; Percentage: percentage change of the values of the variable. | |
Deadband value | DeadBandValue | (only for the Value change sampling mode) Value of the deadband interval. It has priority over the logger deadband general value. For example, if the value is 5, the logger samples the variable only if it has had an absolute or percentage change of at least ± 5 with respect to the previous sampling. |
Provide Feedback