My Entitlements

This section shows a list of the user trials and the user entitlements. For this release the user entitlements tab is disabled.
Both user trials and user entitlements are assigned to a specific user and can be exclusively used by the assigned user in all the organizations which the user has access to.
The user trials or entitlements do not need to be allocated to an organization. A user trial is assigned to the user who redeems the trial via a link shared with them by Rockwell Automation sales representatives.
Free user trial entitlement screen
Once redeemed, the trail appears on the
My Entitlements
page.
Trial user entitlement in the My trials tab
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal