Insert a code snippet

Code snippets are predefined blocks of code for inserting into a structured text program.
To insert a code snippet
  1. In the structured text language editor, put the cursor where you want to insert a snippet.
  2. Enter the keyword for the snippet, and then select the snippet from the prompt list or select
    Tab
    .
    You can also drag a snippet from
    Toolbox
    or double-click it to insert it at the cursor's location in the language editor.
    ST code snippet
  3. Fill in the parameters for the snippets.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal